Skip to main content

Product news – Vienna, 4 April 2024

In Daikin's 100th anniversary year, the Japanese manufacturer is launching the next generation of the high-end Perfera residential air conditioner. The wall-mounted indoor unit has been completely redesigned and reengineered, promising unparalleled benefits for consumers. Year-round climate control and air purification go hand-in-hand with savings due to its market-leading energy efficiency and performance in both low and high ambient temperatures.

Advanced technology for every season

In today's world where energy prices continue to soar, efficiency of home applications is a necessity. The new air conditioning series, Daikin Perfera, is characterised by a seasonal energy efficiency ratio (SEER) of up to 9,47, and a seasonal coefficient of performance (SCOP) of up to 5,20. This allows users to enjoy comfort regardless of the season while reducing the energy consumption of the device. Furthermore, the device has an excellent energy class of A+++ in both cooling and heating modes for pair and multi1) combinations.

Elegant design for comfort and efficiency

  • From its discreet design that seamlessly blends into any interior to its European-modern aesthetics combined with smart functionality, the new Daikin Perfera is more than just an energy-efficient air-to-air heat pump – it's a statement of modern living. These benefits come with this wall-mounted unit:
  • Airflow optimization: The smart twin-flap design, together with the Comfort Plus function, precisely direct the airflow, prevent drafts, and ensure an even distribution of warm or cool air in the room.
  • Motion detection sensor: The 2-zone motion sensor adjusts the airflow and operating mode of the device, thus avoiding direct airflow on occupants. Additionally, the device automatically switches to energy-saving mode when an empty room is detected.
  • Heat boost: Perfera’s heat boost feature enables reaching the desired temperature 14% faster than conventional systems.
  • Quiet Operation: Thanks to the newly designed indoor fan, the unit operates at practically inaudible sound levels (reaching 19 dBA2) in silent mode), making the Perfera an ideal solution for urban homes. 
  • Coupled with a low-noise outdoor unit, Perfera is able to deliver high energy efficiency all while staying unnoticed by other residents and neighbours.
  • Night operation mode: This specially designed feature enables adjusting the temperature set point throughout the night, reducing it by 2˚C in heating or raising it by 0.5˚C in cooling. This contributes to lower energy consumption and ensures a comfortable sleep.
  • Convenience through connectivity: The device can be operated remotely via the Daikin Onecta app, which also enables voice-activated control using Google Assistant or Amazon Alexa. The Daikin Onecta app also provides easy-to-use schedules and provides a quick overview of past energy consumption. When the device is registered on the Daikin Stand By Me platform, users have a constant overview of past and upcoming maintenance tasks and can extend the warranty for eligible devices.
  • Clean indoor air: The integrated Daikin flash streamer technology, a titanium apatite deodorising filter, and a silver allergen filter remove dust, allergens and odours. A new feature is the washable dust filter, treated with an active lonpure substance to additionally capture, reduce and remove bacteria and viruses.

Perfecting service and installation

Maximum capacities for classes 20 to 42 have been increased up to 20% for cooling and 30% for heating all while fitting within existing dimension standards, enabling consumers more cost-efficient solutions.

 

As the Perfera units are fully compatible with the recently introduced Daikin DCS Residential tool for installers and service technicians, easy remote monitoring of operations and adjustment of field settings is possible. This saves costs and time for servicing. Furthermore, thanks to remote diagnostics, technicians can already arrive on site with the necessary spare parts and ideally solve the problem during the first visit. Service technicians can access DCS Residential through the Daikin Stand By Me platform. Additionally, practical digital tools such as Daikin 3D or Daikin E-Care are available to them to provide the best possible customer service. 

References and abbreviations:

1) Limited to specific pair and specific multi combinations with 3MXM52A9

2) dB(A) = A-weighted sound measuring system, accounting for the difference in the way the human ear perceives certain frequencies

Copyrights pictures: Daikin Europe

 

About 

100 years Daikin   

The story of Daikin has always been shaped by groundbreaking ideas, technological innovations, and dedicated people. It began in 1924 when the young Japanese engineer Akira Yamada founded an enterprise in Osaka to manufacture aircraft radiators with a 15-member team. Today, 100 years later, the Daikin Industries Ltd. group brings future-proof solutions for heating, cooling, ventilation, air purification, and refrigeration to global markets. More than 96,000 employees in 173 countries continue the company's legacy of leading technologies to advance low carbon heating and cooling, while ensuring the highest level of comfort. In fiscal year 2022 (1 April 2022 – 31 March 2023) the Daikin group achieved € 28.2 billion sales turnover worldwide. 

 

Daikin Europe N.V. 

Daikin Europe N.V. is a subsidiary of the global group Daikin Industries, and the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC&R) technology in Europe, Middle East and Africa. Daikin designs, manufactures, and brings to market a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial, and industrial purposes. To date Daikin Europe has over 13,700 employees across more than 57 consolidated subsidiaries. It has 14 manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. The headquarters of the Daikin Europe group are in Ostend, Belgium. The company was established in 1972, production in Europe started in 1973. 

 

Daikin Airconditioning Central Europe 

Daikin Airconditioning Central Europe was founded in 1999 with headquarters in Vienna, Austria, as a subsidiary of Daikin Europe N.V. The company's portfolio comprises products and solutions for heating, cooling, ventilation, air purification and refrigeration. More than 700 employees and 2,500 partners are responsible for sales and service activities in 16 countries in Central and Eastern Europe (Austria, Albania, Bosnia Herzegovina, Bulgaria, Croatia, Czech Republic, Hungary, Kosovo, Montenegro, Moldova, North Macedonia, Poland, Romania, Serbia, Slovakia and Slovenia). With Your Daikin World at the Vienna headquarters, the HVAC-R industry and the construction sector have access to a modern experience center for co-creating tailor-made solutions for hotels, retail, offices, and large commercial applications. It also includes one out of nine training centers in the region of Daikin Central Europe. 

 

Media contact  

Doris Passler 
Manager Corporate Communications Central Europe 

Daikin Airconditioning Central Europe HandelsgmbH

Lemböckgasse 59/1/1, 1230 Vienna, Austria

T: +43 (0) 664 24 56 444  

M: passler.d@daikin.at

This might also interest you