Skip to main content

Product news – Vienna, 13 June 2024

With the modular water-to-water heat pump system EW*T-Q-X-A1 featuring Daikin scroll compressors the Japanese manufacturer introduces its latest innovation. This solution offers greater flexibility in configuration, allowing desired capacities for comfort heating, space and process cooling, or heat recovery to be achieved by combining smaller units piped together and controlled as a single system. The modular construction simplifies site selection and installation, streamlines the transportation, handling, and positioning of units, ultimately leading to a plug & play solution with the integration of the Daikin Manifold Kit and Pump Module.

Flexible in application

The new water-sourced EW*T-Q-X-A1 heat pumps offer heating or cooling operation under various conditions. They can produce hot water up to +60°C, while chilled water is supplied in the range from -15°C (with a water-glycol mixture) to +30 °C for the evaporator leaving water temperature. Therefore, the range of applications that can be covered is wide, including comfort heating, space and process cooling, heat recovery.

Comprising three base modules with capacities of 100 kW, 125 kW and 160 kW, the range features Daikin scroll compressors and is available in two sound versions. This includes a reduced sound variant suitable for outdoor installation and noise-sensitive applications as condominiums, hotels and hospitals.

Unit configurations by type include:

  • Water-to-water heat pump with inversion on water side
  • Water-to Water heat pump with inversion on refrigerant side (100 kW only)
  • Condenser-less version

Five benefits of modularity

  • Scalability

Thanks to its modularity, the new EW*T-Q-X-A1 offers scalability, reducing initial investment costs and providing the potential for future expansion with additional modules installed when building occupancy increases. The introduction of a common scroll layout ensures greater compatibility, promoting system longevity and making future system upgrades effortless. The modules can be combined in a side-by-side array or stacked to minimise space requirements, which is especially useful for retrofit applications.

 

  • Compactness

Each of the different modules is very compact and can be easily transported and positioned within the installation space. As a single module is 120 centimeters wide, 130 cm centimeters depth and 100 centimeters high, it can be handled with a forklift, eliminating the need of a crane.

 

  • Plug  & play installation

Installation can be further simplified by using the Daikin Manifold Kit, designed to connect modules among each other on the water side,  including the piping. Each Manifold Kit is equipped as standard with manual isolation valves for all connections, allowing each individual module to be excluded from the circuit in case of maintenance without needing to stop the entire system.

Additionally, a dedicated Pump Module can be easily added to the array of modules. The Pump Module is equipped with inverter pumps for full flexibility and includes an expansion tank with a volume of 18 liters.

 

  • Lower operating costs

Thanks to its modular design, the new EW*T-Q-X-A1 can closely follow the cooling and heating load profile of the building compared to packaged chillers, significantly improving the efficiency. This is particularly relevant as it ensures lower operating costs for the modular design HVAC system under part load conditions, which represent the majority of the operational time.

  • Outstanding energy performance with limited environmental impact

Daikin is committed to continuous design improvement aimed at reducing the environment impact of its cooling, heating and refrigeration solutions. Daikin Bluevolution heat pumps and chillers use R-32 refrigerant which has a Global Warming Potential (GWP) of 675, just one third of R-410A. This, combined with high-energy efficiency, has the potential to substantially reduce a building’s carbon footprint substantially. Additionally, the reduction in required refrigerant charge enabled by the use of R-32 offers further efficiencies while reducing installation and service costs.

The modular water-to-water heat pump system EW*T-Q-X-A1 is available in the CE-region since April 2024. For more information visit the product informtion at EWWT-Q / EWHT-Q / EWLT-Q | Daikin.

 

 

Photo copyrights: Daikin Europe

About

100 years Daikin  

The story of Daikin has always been shaped by groundbreaking ideas, technological innovations, and dedicated people. It began in 1924 when the young Japanese engineer Akira Yamada founded an enterprise in Osaka to manufacture aircraft radiators with a 15-member team. Today, 100 years later, the Daikin Industries Ltd. group brings future-proof solutions for heating, cooling, ventilation, air purification, and refrigeration to global markets. More than 98,000 employees in 175 countries continue the company's legacy of leading technologies to advance low carbon heating and cooling, while ensuring the highest level of comfort. For its fiscal year 2023 the global Daikin group reported a record sales result of € 28 billion sales (1 April 2023 – 31 March 2024). 

Read more on 100 Years Daikin

 

Daikin Europe N.V. 

The Daikin Europe group is the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, Middle East, and Africa. Daikin designs, manufactures, and offers customers a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial, and industrial purposes. To date, Daikin Europe has over 13,800 employees across more than 59 subsidiaries. It has 14 manufacturing sites in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. Headquartered in Ostend (Belgium) for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries. 

Read more on www.daikin.eu

 

Daikin Airconditioning Central Europe

Daikin Airconditioning Central Europe was founded in 1999 with its headquarters in Vienna, Austria, as a subsidiary of Daikin Europe. Its portfolio comprises products and total solutions for heating, cooling, ventilation, air purification, and refrigeration needs in residential, commercial, and industrial settings. More than 700 employees and 3,400 partners are responsible for sales and service activities in 16 countries in Central and Eastern Europe, including Austria, Albania, Bosnia and Herzegovina, Bulgaria, Croatia, the Czech Republic, Hungary, Kosovo, Montenegro, Moldova, North Macedonia, Poland, Romania, Serbia, Slovakia, and Slovenia.

With "Your Daikin World" at the Vienna headquarters, and the “Daikin Inspiration Park” the HVAC-R industry and the construction sector have access to two modern B2B-experience centers for co-creating tailor-made solutions for hotels, retail, offices, and large commercial applications. Across the CE-region Daikin runs 10 out of 116 B2B-trainings centers across Europe. Consumers and homeowners receive consulting in four B2C-Experience centers in Vienna, Belgrad, Bratislava and Budapest.

Read more on www.daikin-ce.com

 

Media contact

Doris Passler
Manager Corporate Communications Central Europe

Daikin Airconditioning Central Europe HandelsgmbH

Lemböckgasse 59/1/1, 1230 Vienna, Austria

T: +43 (0) 664 24 56 444

M: passler.d@daikin.at

This might also interest you